2012-09-04 5:41 AM
I have been developing some applications for the STM8S103F3 which I have on breadboard and I have recently transferred one of the projects to the STM8S Discovery board and I am finding a difference in behaviour which I cannot work out.
The program uses PWM Mode 2 to output a 60 uS square wave on timer 1 channel3. On the STM8S103F3 on breadboard the program works fine and I get a 0 to 3.3V square wave.On the Discovery board I have the square wave with the right frequency but the output voltage is only 280 mV peak-to-peak. The only things I have connected to the Discovery board are the USB connection and the scope connected to the timer output and ground.I am using IAR as the development environment and I have modified the include files and project options accordingly.Any ideas where I could be going wrong? Am I correct in assuming that if the app runs on the STM8S103F3 then it will run on the Discovery board assuming I change the include file and target chip?The code for the application is included below.Regards,Mark&sharpinclude <intrinsics.h>&sharpinclude <iostm8s103f3.h>//// Setup the system clock to run at 16MHz using the internal oscillator.//void InitialiseSystemClock(){ CLK_ICKR = 0; // Reset the Internal Clock Register. CLK_ICKR_HSIEN = 1; // Enable the HSI. CLK_ECKR = 0; // Disable the external clock. while (CLK_ICKR_HSIRDY == 0); // Wait for the HSI to be ready for use. CLK_CKDIVR = 0; // Ensure the clocks are running at full speed. CLK_PCKENR1 = 0xff; // Enable all peripheral clocks. CLK_PCKENR2 = 0xff; // Ditto. CLK_CCOR = 0; // Turn off CCO. CLK_HSITRIMR = 0; // Turn off any HSIU trimming. CLK_SWIMCCR = 0; // Set SWIM to run at clock / 2. CLK_SWR = 0xe1; // Use HSI as the clock source. CLK_SWCR = 0; // Reset the clock switch control register. CLK_SWCR_SWEN = 1; // Enable switching. while (CLK_SWCR_SWBSY != 0); // Pause while the clock switch is busy.}//// Initialise Timer 1.//void InitialiseTimer1(){ TIM1_CR1 = 0; TIM1_CR2 = 0; TIM1_SMCR = 0; TIM1_ETR = 0; TIM1_IER = 0; TIM1_SR2 = 0; TIM1_CCER1 = 0; TIM1_CCER2 = 0; TIM1_CCMR1 = 0; TIM1_CCMR2 = 0; TIM1_CCMR3 = 0; TIM1_CCMR4 = 0; TIM1_CCER1 = 0; TIM1_CCER2 = 0; TIM1_CCMR1 = 0; TIM1_CCMR2 = 0; TIM1_CCMR3 = 0; TIM1_CCMR4 = 0; TIM1_CNTRH = 0; TIM1_CNTRL = 0; TIM1_PSCRH = 0; TIM1_PSCRL = 0; TIM1_ARRH = 0; TIM1_ARRL = 0; TIM1_CCR1H = 0; TIM1_CCR1L = 0; TIM1_CCR2H = 0; TIM1_CCR2L = 0; TIM1_CCR3H = 0; TIM1_CCR3L = 0; TIM1_CCR4H = 0; TIM1_CCR4L = 0; TIM1_OISR = 0; TIM1_EGR = 0x01; TIM1_DTR = 0; TIM1_BKR = 0; TIM1_RCR = 0; TIM1_SR1 = 0;}//// Set up Timer 1, channel 3 to output a single pulse lasting 30 uS.//void SetupTimer1(){ TIM1_ARRH = 0x03; // Reload counter = 960 TIM1_ARRL = 0xc0; TIM1_PSCRH = 0; // Prescalar = 0 (i.e. 1) TIM1_PSCRL = 0; TIM1_CR1_DIR = 0; // Up counter. TIM1_CR1_CMS = 0; // Edge aligned counter. TIM1_RCR = 0; // No repetition. // // Now configure Timer 1, channel 3. // TIM1_CCMR3_OC3M = 7; // Set up to use PWM mode 2. TIM1_CCER2_CC3E = 1; // Output is enabled. TIM1_CCER2_CC3P = 0; // Active is defined as high. TIM1_CCR3H = 0x01; // 480 = 50% duty cycle (based on TIM1_ARR). TIM1_CCR3L = 0xe0; TIM1_BKR_MOE = 1; // Enable the main output.// TIM1_CR1_OPM = 1; TIM1_CR1_CEN = 1;}//// Main program loop.//void main(){ // // Initialise the system. // __disable_interrupt(); InitialiseSystemClock(); InitialiseTimer1(); SetupTimer1(); __enable_interrupt(); while (1) { __wait_for_interrupt(); }} #stm8s103f3-discovery-timer2012-10-06 2:37 AM
Worked this one out (with the help from a friend). The problem is that the pin outputting the Tim1Ch3 signal is connected to the touch sensor. I changed the channel to Tim1Ch4 and everything is looking good.
I could have removed the connection as the manual tells you how to do this but I thought I'd try the non-invasive route first.Regards,Mark2017-07-04 4:38 AM
hi,
I am having a similar issue with Timer 2, channel 2 on Port D Pin 3.
I've double checked the schematic fir the STM8S discovery board and this pin is unused.
My timer configuration is as follows:
void TIM2_PWM(void)
{ /* SET PRESCALER */ TIM2.PSCR = 0; /* SET ARR */ TIM2.ARRH = 0x4E; TIM2.ARRL = 0x1F; /* CH1 ENABLED ACTIVE LOW POLARITY */ TIM2.CCER1 = 0x30; /* PWM2 */ TIM2.CCMR2 = 0x70; /* SET PULSE WIDTH */ TIM2.CCR2H = 0x3E; TIM2.CCR2L = 0x80; /* ENABLE PRELOAD REGISTER */ TIM2.CCMR2 |= 0x08; /* TIM2_ARR PRELOAD ENABLE */ TIM2.CR1 |= 0x80; /* TIM2 ENABLE */ TIM2.CR1 |= 0x01;}The resulting output is generating a 800Hz signal with a 80% duty cycle, as desired. However, the waveform is peaking at 360mV. I have that pin configured as a push-pull output at 10Mhz.
Any help would be greatly appreciated.
Regards
Aaron
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.