2019-08-22 1:47 AM
Hello,
I am trying to rebuild STM8A discovery project(AN4101). After building I got the error ''#error clnk Debug\stm8af_discover.lkf:1 @svlreg missing for function f_CAN_RX_IRQHandler''. Similar post about this issue were answered as write '@svlreg' before interrupt function but the code I run belongs to ST and I don't know where to find interrupt function to write @svlreg before it.
Thanks for attention.
2019-08-22 3:45 AM
Solved.
2020-01-09 1:24 AM
Hello Voneparte
Could you let me share the solution resolved ?
I'm in the similar problem, " #error clnk Debug\eeorc_0_8_pjt.lkf:1 @svlreg missing for function f_TIM2_UPD_OVF_TRG_BRK_USART2_TX_IRQHandler"
I checked and just guess the error is caused as a result whether the function specified (like size ...) is inserted(called) or not in the Handler.
Thanks in advance
--------------------------------------------------------------------------------------
INTERRUPT_HANDLER(TIM2_UPD_OVF_TRG_BRK_USART2_TX_IRQHandler, 19)
{
switch (SYS_Mode)
{
case SYS_RUN:
this function is cause -> Sys_Run_ftn(); // this function is blocked, no error,
break;
case SYS_TEST:
Sys_Test_ftn(); // This is always OK.
break;
default:
break;
}
TIM2_ClearITPendingBit(TIM2_IT_Update);
enableInterrupts();
}
2020-01-09 5:32 PM
I had fixed this issue with converting from 32 bits parameter to 16 bits the length of some parameters used in sub-function (second depth in my case ). But there's alternative solution , just adding "@svlreg" in the front of the function name.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.