cancel
Showing results for 
Search instead for 
Did you mean: 

SVF file format

aberracasa
Associate II
Posted on June 07, 2004 at 15:02

SVF file format

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
aberracasa
Associate II
Posted on May 17, 2011 at 12:01

Hello,

I need to program a UPSD3234BV part in system via the JTAG port. As with other ISP devices, I generated a SVF file from the OBJ. I have the following questions:

1. While I understand the functionality of TERR and TSTAT I cannot see how the 2 SVF files (4-pin vs 6-pin) are to be used differently.

2. The SVF files are HUGE. I noticed that the programming is done in 11-bit chunks. Is there a way to create a smaller SVF file, a binary SVF file? I am trying to fit it into the system controller's FLASH.

Thank you,

Andre
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.