2017-04-26 4:58 AM
Hi,
I've been trying to connect my application through ST-LINK according to the
, but when I invokeESelectHard('ST-LINK', 'SWIM', FALSE)
it returns 0, and
CGetLastError
provides the following message:File \TOOLS.CNF : No such file or directory
The file TOOLS.CNF is clearly present in the same directory as the .dll files that I successfully manage to load (eprcore60.dll, dbca60.dll, lef60.dll and file60.dll).
What is the policy of s
2017-04-26 5:02 AM
I accidentally sent the incomplete question and can't find a way to edit it.
I wanted to ask, what is the policy of searching for the .cnf files in the file60.dll -- are the paths hard coded, or are they relative to the dll files, or can their path be set somehow?
I enclose the complete source code of my attempts below:
#include 'stdafx.h'
#include <windows.h>
#include <conio.h>
#ifndef MAX_PATH
#define MAX_PATH 260
#endif // MAX_PATH
using namespace std;
#define WARN(msg, ...) fprintf(stderr, msg '\n', ## __VA_ARGS__)
#define WWARN(wmsg, ...) fwprintf(stderr, wmsg L'\n', ## __VA_ARGS__)
typedef int(*EAllAccess_t)(DWORD dwAreaId);
typedef int(*EAreaAccess_t)(DWORD dwAreaId, long FirstAddr, long LastAddr);
int(*ESelectDevice)(const char *szDevice);
int (*ESelectHard)(const char *szCard, const char *szProtocol, BOOL bDemo);
int(*ESelectPort)(const char *szPort);
int(*ESetPreferences)(int iPreference, BOOL bState);
int(*ESetProtection)(const char *szProtectMode, BOOL bState);
int(*ECheckSum)(DWORD dwAreaId, long *FileCheckSum, long *MemoryCheckSum);
int (*EGetId)(const char *szName, DWORD *pdwId);
char *(*EGetImagePtr)(DWORD dwAreaId, long *MemSize);
int(*ECloseComm)();
char *(*CGetLastError)() = NULL;
char *LastErrorMessage()
{
if (CGetLastError)
{
return CGetLastError();
}
return 'unknown error';
}
#define TRY(action) if(!(action)) { WARN(# action ' failed: %s', LastErrorMessage()); return; }
EAllAccess_t EBlankAll;
EAreaAccess_t EBlankArea;
EAllAccess_t EEraseAll;
EAreaAccess_t EEraseArea;
EAllAccess_t EProgAll;
EAreaAccess_t EProgArea;
//EAllAccess_t EReadAll;
EAreaAccess_t EReadArea;
EAllAccess_t EVerifyAll;
EAreaAccess_t EVerifyArea;
void LoadLibraries()
{
HINSTANCE eprcore, dbca, lef, file;
TRY(eprcore = LoadLibrary(L'eprcore60.dll'));
TRY(dbca = LoadLibrary(L'dbca60.dll'));
TRY(lef = LoadLibrary(L'lef60.dll'));
TRY(file = LoadLibrary(L'file60.dll'));
TRY(CGetLastError = (char *(*)()) GetProcAddress(dbca, 'CGetLastError'));
TRY(ESelectPort = (int(*)(const char *))GetProcAddress(eprcore, 'ESelectPort'));
//TRY(EReadAll = (EAllAccess_t)GetProcAddress(eprcore, 'EReadAll'));
TRY(ESelectHard = (int(*)(const char *, const char *, BOOL)) GetProcAddress(eprcore, 'ESelectHard'));
TRY(EReadArea = (EAreaAccess_t)GetProcAddress(eprcore, 'EReadArea'));
TRY(EVerifyAll = (EAllAccess_t)GetProcAddress(eprcore, 'EVerifyAll'));
TRY(EVerifyArea = (EAreaAccess_t)GetProcAddress(eprcore, 'EVerifyArea'));
TRY(EProgAll = (EAllAccess_t)GetProcAddress(eprcore, 'EProgAll'));
TRY(EProgArea = (EAreaAccess_t)GetProcAddress(eprcore, 'EProgArea'));
TRY(EEraseAll = (EAllAccess_t)GetProcAddress(eprcore, 'EEraseAll'));
TRY(EEraseArea = (EAreaAccess_t)GetProcAddress(eprcore, 'EEraseArea'));
TRY(EBlankAll = (EAllAccess_t)GetProcAddress(eprcore, 'EBlankAll'));
TRY(EBlankArea = (EAreaAccess_t)GetProcAddress(eprcore, 'EBlankArea'));
}
void ReadMemory()
{
DWORD PROGRAM_MEMORY, DATA_MEMORY;
TRY(ESelectHard('ST-LINK', 'SWIM', FALSE));
TRY(ESelectDevice('STM8L15xC6'));
TRY(ESelectPort('USB'));
TRY(EGetId('PROGRAM MEMORY', &PROGRAM_MEMORY));
TRY(EGetId('DATA MEMORY', &DATA_MEMORY));
WARN('PROGRAM MEMORY = %d, DATA MEMORY = %d', PROGRAM_MEMORY, DATA_MEMORY);
}
int main()
{
TCHAR pwd[MAX_PATH];
_wgetcwd(pwd, MAX_PATH);
WWARN(L'Current Working Directory: %s\n', pwd);
SetDllDirectory(L'C:\\st_toolset\\stvp');
LoadLibraries();
ReadMemory();
getchar();
return 0;
}
2017-04-26 7:19 AM
I managed to solve the problem by invoking the 'CSetWorkingDir' function. Sorry for the noise.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.