2007-01-22 10:07 PM
STR912F44W CAN receiver not working
2011-05-17 12:35 AM
hi Softy,
>CAN-TX on port 5.1 is working (in Loopback-mode) but the receiver is not working in all modes Can you send the configuration (CAN and GPIO)you're using ? it seems that the GPIO configuration is not right because the loopback-mode is working ;) Waiting for your response best regards. :D2011-05-17 12:35 AM
The problem is: STR912F44W CAN node in silent-mode.
CAN-TX on port 5.1 is working (in Loopback-mode) but the receiver is not working in all modes - also not in silent mode. FI2 is selected for RX buffer. Acceptance filter is set to the full range like the example does. Interrupt is enabled scu on port 5 is enabled - but no int occures. Any ideas? :oWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.