2006-08-30 10:46 PM
2011-05-17 12:30 AM
I notice that all the ST examples using IAR compiler use the following to configure the bank0/1 sizes/addresses at reset.
; --- Remap Flash Bank 0 at address 0x0 and Bank 1 at address 0x80000, ; when the bank 0 is the boot bank, then enable the Bank 1. LDR R6, =0x54000000 LDR R7, =0x4 <== should be 6 STR R7, [R6] LDR R6, =0x54000004 LDR R7, =0x3 <== should be 2 STR R7, [R6] LDR R6, =0x5400000C LDR R7, =0x0 STR R7, [R6] LDR R6, =0x54000010 LDR R7, =0x20000 <== should be 0x80000 STR R7, [R6] LDR R6, =0x54000018 LDR R7, =0x18 STR R7, [R6] looking at the register description and comments i get the different values for the config above. Config above is for a STR91xFx44 device. Could someone confirm i am correct or misreading the ref manual. Regards sjo2011-05-17 12:30 AM
The manual is not very clear on those point
LDR R6, =0x54000000 LDR R7, =0x4 <-- This correct because bootBank size is 64K * 2^0x4 = 512K STR R7, [R6] LDR R6, =0x54000004 LDR R7, =0x3 <== should be 2 <- So far I understand, You are righ 8K * 2^2 = 32K STR R7, [R6] LDR R6, =0x5400000C LDR R7, =0x0 STR R7, [R6] LDR R6, =0x54000010 LDR R7, =0x20000 <== should be 0x80000 <-- NO the address are specifed in 4 bytes word STR R7, [R6] LDR R6, =0x54000018 LDR R7, =0x18 STR R7, [R6] Regards2011-05-17 12:30 AM
Hi acorchia, Sjo,
I agree with you , the flash configuration section is not very clear in reference manual. The correct flash configuration when Bank0 is the boot bank is: LDR R6, =0x54000000 LDR R7, =0x4 -> BootBank size is: 32K * 2^0x4 = 512K STR R7, [R6] LDR R6, =0x54000004 LDR R7, =0x2 -> NonBootBank size is: 8K * 2^2 = 32K STR R7, [R6] ** 0x3 was used in the IAR example because there is an issue with rev B of STR9 where you need to configure Bank1 as 64K , but for rev D and later, you need to put 0x2 (please refer to STR9 errata sheet v2.0 paragraph 2.1 for more details). LDR R6, =0x5400000C LDR R7, =0x0 -> boot bank address: 0X0 STR R7, [R6] LDR R6, =0x54000010 LDR R7, =0x20000 *** STR R7, [R6] *** non boot bank address : 0x80000, but it should be shifted by 2 because Flash bus address A[23:0] is connected to CPU bus address A[25:2]. LDR R6, =0x54000018 LDR R7, =0x18 -> enable banks STR R7, [R6] Best regards, STARMWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.