2009-03-22 10:06 PM
2011-05-17 12:58 AM
Dear All,
We are working on STR9 - IAP. For changing Boot Bank order & loading IAP driver we are using RFlasher. Then we uses ST Flash Loader for programming Application in Bank0 through UART0. Uptill this everything is OK. But Aplication is not running. If we want to reorder the Boot Banks, how should we do it ? Presently we are not getting any setting in RFlasher for it.2011-05-17 12:58 AM
Hi,
Please see this thread on the Raisonance forum: http://raisonance-forum.xsalto.com/viewtopic.php?id=2741 That will tell you how to configure RFlasher for programming the Configuration, and the CSX bit that is inside it. Best Regards, Vincent2011-05-17 12:58 AM
Thank You, VincentC,
Now I am able to programme & boot required bank if I programmed those from Rflasher. :D I downloaded my Application in Bank0 through JTAG & after that ST IAP driver in Bank1 ( with booting from it ). Now whenever STR9 boots, firat it runs IAP driver. If push button is not pressed, it starts Application Code correctly. :D If push button is pressed then it start UART programming mode. I also abled to download application code through STFlasher & UART. ST Flasher ''Invalid Address'' error , if I doanloadhex file in it. :-[ Therefore I converted same hex file to bin & downloaded it through ST Flasher & UART successfully, but when I restarts STR9 after it, application code doesn't works . :-[ What should be done for it ? Please help, Sachin Bhujbal [ This message was edited by: s_bhujbal on 23-03-2009 10:37 ] [ This message was edited by: s_bhujbal on 23-03-2009 10:38 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.