2006-04-10 8:19 PM
2006-03-23 1:57 AM
Hello,
I want to use you IAP-Driver for Downloading Software to the ARM-Controller. The IAP-Driver worked correctly. But I the application program won´t wort at starting adress 0x40002000. I use the Keil Compiler. Can you give some information about remapping the Interruptvectors to ram adress 0 and to reserve this region for the vectors. Can you give me some information. Thanks maenni2006-03-23 6:23 AM
Hi,
Unfortunately I can't help you with this (yet) as I'm just trying to acquire/build the IAP for the STR71x and Keil uVision3 toolchain. Where did you get the IAP code? Did you have to manually create the Keil project and import all of the relavent files, etc? How did you get started? Thanks, Steve2006-03-23 7:06 AM
Hi,
I get this file from the ST-download side. I compiled it with the RV-Development-Kit. I have created the project manually. I got an update from the Keil compiler for the RVD. You have to insert the scatter file in the linker menu. then it should will work. hope this will help you maenni2006-03-23 7:52 AM
HI,
I created the project manually. You have to include the scatter file in the project menu for the linker. After doing this the program should work. I can download files with the Hyper-terminal without any problems. The only problem is my application at 40002000H. I have created my own application with the Keil C-Compiler and I don´t know how I can remap the interrupt-vectors so that my application runs. I hope this may help you maenni2006-03-30 7:16 PM
Hi,
I am using ADS,as maenni said,how can I preserve space for interrupt vectors in preliminary ram space when mapping ram at 0x00 in case that ZI area for c code inhabit here? thanks oolalaWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.