cancel
Showing results for 
Search instead for 
Did you mean: 

STR710 interrupt with P1.15

rekisum
Associate II
Posted on September 20, 2006 at 07:52

STR710 interrupt with P1.15

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
rekisum
Associate II
Posted on September 20, 2006 at 07:12

Hi,

in the data sheet pin P1.15 of the STR710 is marked as an interrupt input.

In the reference P1.15 is not listed in the XTI list. :o

So i wonder if and how I can use P1.15 as interrupt input.

Maybe there is a trick with the HDLC module?

Regards,

Joerg

ewitt
Associate II
Posted on September 20, 2006 at 07:37

In my

http://www.st.com/stonline/books/pdf/docs/10350.pdf#search=''STR71x'';

P1.15 is not marked as interrupt input at all...

So no wonder that it is not in the XTI list.

rekisum
Associate II
Posted on September 20, 2006 at 07:52

:(

Yes they changed it:

'22-May-2006: removed x in interrupt column

for P1.15 and P1.12 in Table 3 and Table 6'

I got the datasheet from oktober 2005!

That sucks!

Thanks anyway....

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.