2008-07-14 2:25 PM
2008-06-27 11:12 AM
Has anyone managed to get an interrupt driven I2C handler working, with error recovery for events such as bus errors or non-existent device? The ST example for I2C is woefuly inadequate, and the STR750 manual has virtually no information on how to recover from errors, especially a bad device address (a common occurence when enumerating devices on a common bus).
Ad hoc experiemnting shows that the AF flag is sometimes set (SR1 = 0x10, SR2 = 0x92) when a device does not respond, but this doesn't seem to happen consistently. At times I get both SR1 and SR2 set to zero in interrupts, no idea how this happens since there's no interrupt source. It doesn't occur when a valid device is found. Perhaps there's some errata on the I2C bus?2008-07-14 2:25 PM
I was wondering whether you got you ISR based I2C communications to work.
I have implemented an ISR to track I2C errors. I've been trying to debug this but I am not seeing the issue. Here is my ISR functionCode:
void RmiOverI2c::I2cISR(void) { g_uStatus = I2C_GetStatus(I2C1); I2C_FlagClear (I2C1, I2C_EVF); if(g_uStatus & I2C_AF) { CI2c_Pulse(10) I2C_FlagClear (I2C1, I2C_AF); } else if(g_uStatus & I2C_BERR) { CI2c_Pulse(20) } else if(g_uStatus & (I2C_AF | I2C_BERR)) { CI2c_Pulse(15) } } The ISR routine is being called from a standard IAR IRQHandler in 71x_vect.s. My problem is that the EVF won't clear even though I2C_GetStatus() accesses CR, SR1 and SR2 which is suppose to clear most if not all flags according to the STR711 reference. I watch the registers for I2C1 and do not see any changes. Thanks, J.R.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.