2013-03-23 11:16 PM
I've working with the STM8S103K3T6C (LQFP package) and getting SPI Master working, without the Standard Peripheral libraries. I am able to send data correctly, however I havn't been able to get the hardware SPI peripheral to manage the CS/SS line for me. No combination of the SPI_CR2_SSM and SPI_CR2_SSI registers seems to work. I've tried both the default NSS pin (PE5) and the optional NSS pin (PA3) with the correct AFR bit set. What do I need to do to enable hardware management of CS/SS?
#spi-nssWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.