2008-03-13 4:50 AM
Startup File, 91x_it.c, Undefined_Handler
2011-05-17 12:50 AM
Hello.
I'm working with Keil uVision and the ST-Library V2.0. My application is loaded in Bank 0 and I want to use Bank1 storing data in flash. The examples of Keil for flash read/write doesn't run, My Startup-File: STR91x.S If you want store data in flash, the following assembler code is needed: MOV r0, #0x40000 MCR p15,0x1,r0,c15,c1,0 This code is in 91x_init.s. I made a own startup-file and modified STR91x.s with the assembler code for flash read/write. But now I have the problem, that i get sometimes an Undefined_Handler() and my application doesn't continue to run. My question: Which startup-file (STR91x.s or 91x_init.s) shall I use with the ST-Lib and Keil uVision? Why is in 91x_it.c in Undefined_Handler() an infinite loop and how treat such an Handler. I dont see the cause for the undefined_Handler with the debugger. How can I find out, why it jumps to Undefined_Handler? ThomasWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.