2006-08-29 11:49 AM
2011-05-17 12:31 AM
Does anybody have a simple Startup- and linker file for the GNU-Compiler?
Maybee with a smal c-Programm? regards ED2011-05-17 12:31 AM
The Hitex HITOP for arm has an example of gcc for str9.
You can download the demo version where you can find the demo for str9. The has a GCC toolchain with some demo for STR9. I attached the demo project for Hitex where you can find startup.s and linker file. I suggest you to compared the startup.s file with the iar one. some initialization in the gcc version are missing like: #ifdef BUFFERED_Mode ; BUFFERED_Mode ; ------------------------------------------------------------------------------- ; Description : Enable the Buffered mode. ; When enable, just enable the buffered define on the 91x_conf.h ; ; ------------------------------------------------------------------------------- MRC p15,0,r0,c1,c0,0 ; Read CP15 register 1 into r0 ORR r0, r0, #0x8 ; Enable Write Buffer on AHB MCR p15,0,r0,c1,c0,0 ; Write CP15 register 1 #endif ; --- Remap Flash Bank 0 at address 0x0 and Bank 1 at address 0x80000, ; when the bank 0 is the boot bank, then enable the Bank 1. LDR R6, =0x54000000 LDR R7, =0x4 STR R7, [R6] LDR R6, =0x54000004 LDR R7, =0x3 STR R7, [R6] LDR R6, =0x5400000C LDR R7, =0x0 STR R7, [R6] LDR R6, =0x54000010 LDR R7, =0x20000 STR R7, [R6] LDR R6, =0x54000018 LDR R7, =0x18 STR R7, [R6] ; --- Enable 96K RAM LDR R0, = SCRO_AHB_UNB LDR R1, = 0x0196 STR R1, [R0] ; --- Reset VIC controller LDR R0, = SCR0_AHB_PER_UNB LDR R1, [R0] ORR R1, R1, #VIC_RES_BIT STR R1, [R0] ; --- Disable any source of interupt // used in debug mode LDR R0, = VIC0_BASE LDR R1, =0xFFFFFFFF STR R1, [R0, #VICx_INTECR] LDR R0, = VIC1_BASE STR R1, [R0, #VICx_INTECR]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.