2008-05-14 11:30 PM
(ST9PlusV6.2.0) GNU compiler problem?
2011-05-17 2:32 AM
While debugging my project I have discovered the following behavior which does not make sense to me. I am hoping that maybe someone out there may see the reason for the problem and could give me a hint or a solution.
The following code sniped reads like this in C… m_nValue += m_nValue; and like this in the .lst file (listing). ldw rro,#@m_nValue addw @m_nValue+2,2(rr0) adcw @m_nValue,(rr0) m_nValue is a static long variable and it is also #pragma REGISTER_FILE m_nValue For example, if I initialize m_nValue with 0 the output after the += function is not 0 as suggested. The output can be anywhere in the 32bit range. The output value is always the same for a compilation. If I change code and recompile the output variable is different than before. My compile options look like this: -m$(MODEL) -mfp-on -I$(INCDIR) -O1 -Wall -c -Wa,-alhd=$*.lis I am using the MODEL: medium. Any suggestions are highly appreciated.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.