2002-11-25 11:11 AM
2011-05-17 2:32 AM
what headers/connections are required from me on my ST92F150 controller
board in order to perform in circuit programming ? Skywalker2011-05-17 2:32 AM
ICP is used wiith the ST7, the ST9 uses the In System Programing (ISP).
Refer to the datasheet for details on this protocol based on a synchronous communication at reset using the SCI-M. The connector needed is described in the EPB User Manual that you can find on this site (http://www.stmcu.com/mdtfiles/989589078.pdf).2011-05-17 2:32 AM
6 pins is all you need once you have removed the unnecessary NC and GND pins.
By the way, more information on ISP is available on the AN1450 application note (ST9 Flash Programming). Regards, Jojo [ This message was edited by: jojo on 26-11-2002 00:41 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.