2014-03-27 12:09 PM
Hi,
I'm trying to use the ST Visual Develop with the Cosmic st8 32k compiler. I install everything and build the project. That all works fine. When I try to connect to the Discovery board with the debugger using Swim ST-link, I receive the following error:Starting debug session...-> Emulator reset (usb://usb)...
** Connection error (usb://usb): gdi-error [40201]: can't access configuration database
-> Failed to connect target.I have tried uninstalling and re-installing everything including the drivers. I've tried other target settings. The only one that works is the simulator.When I connect the Discovery board, my computer sees it as an external HD. I get the pop-up window and can look at the links stored on the board. I'm using Windows 7 64bit.I should also add that after the above error message a windows 7 pop-up appears saying that gdb7 has stopped working and a red LED glows on the board.Any help would be appreciated.Regards,Marc #stm8-discovery #i-also-get-same-error-so-please
2019-11-27 8:37 PM
Hi there. I am facing same issue. Did you find any fix?
2019-11-27 9:02 PM
Thanks a lo0ot. This worked for me. Only one thread on google which is talking about this issue.
2019-12-04 8:43 AM
Running 'ST Toolset.msi' did not work for me (both as normal user and admin) but I found my solution here:
https://community.st.com/s/question/0D50X00009XkXhpSAF/stlink-v2-configuration-database
It says:
You will need to open a command prompt in administrator mode. For those that don't know you will find it at
Windows/Start button->All Programs->Accessories->
Right click on 'Command prompt' and select 'run as administrator'
First type this one
Regsvr32 /u "C:\Program Files (x86)\Common Files\Microsoft Shared\DAO\DAO350.DLL"
And then this one
Regsvr32 "C:\Program Files (x86)\Common Files\Microsoft Shared\DAO\DAO350.DLL"
This unloads and then reloads the DAO DLL which fixes the problem nicely. It also assumes you have a standard install of Windows so if you put DAO350.DLL somewhere else then you will have to change the paths.
You might also have to cd \windows\system32 before anything to use regsvr32 but mine defaults to there
@jwilson @MRaja.1710 @Ilia Baranov
2019-12-19 10:38 PM
Hello
I'm facing too. Could you let me know the method if you fixed ?
2019-12-19 10:49 PM
Did you find the solution ?
2019-12-23 8:25 PM
The above answer from Mworl.1974 (Community Member) solved my issue.
2019-12-23 9:29 PM
Thanks, the issue was fixed.
2020-01-02 5:54 AM
I tryed everything above and the same error appear and appear and not resolve, i don´t know more, i am thinking that ST have a big problem with this and everyone have the same situation and not resolved, what can i do to resolve?????????
2020-06-12 9:20 PM
hi every one ,,
if you don't get solution for the same
for windows 10 press windwos+x and select admin power sell
and type this two command
best regard,
sachin patel
2020-09-16 4:22 AM
I tried the STtoolset.msi repair - not fixed
Did an uninstall / reinstall - fixed it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.