2007-04-05 10:19 PM
ST7ULTRALITE INTERNAL RC OSCILLATOR
2007-04-05 10:07 PM
The predefined calibration low byte value of rc calibration for 5V(RCCRL0) is located in 0xDDE1, but what is its format?
The 2 bits CR0-CR1 where are locate? Thank you in advance for help.2007-04-05 10:19 PM
Hi,
They are located on bit 5 and 6, so you don't need to perform any shift to copy them in SICSR register. You have to take care about : - LVDRF bit which will be cleared by reading the SICSR register, so this check must be performed before setting the RC calibration or the SICSR register must be saved in a variable. - AVDIE : which will be clear if you don't mask it For more information about SICSR, refer to datasheet. Best regards LaurentWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.