2007-05-31 11:46 PM
2007-05-31 8:44 PM
Hello together!
I have a problem with the configuration with the oszillator setup. I want to start the MCU with 8Mhz on the fcpu. I need the Pll and the CPU voltage about 5VDC. The MCO will be enabled with 4 MHz. I write the Code in C. I can't find the option bytes for the Pll. Can you help me please?2007-05-31 11:46 PM
If I understand the meaning of your post, you want to clock the ST7FLITE39 from an external crystal that resonates at 8 MHz.
If it is true, the MCO pin should output a 4 MHz square wave, since the signal from the crystal attached to OSC1 and OSC2 is divided by 2 (see Figure 13, page 25 of datasheet). To have fcpu = 8 MHz, you have two options: use a 16 MHz crystal, or use the internal RC oscillator and the PLLx8. All these setup options are encoded in the flash options bytes that are shown at pages 162-163 of the datasheet. To change these settings, you need only to check some option in your programming device. Regards EtaPhiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.