2007-09-28 3:21 AM
2007-09-27 8:27 PM
Hi,
I have a problem with the linker and the files .lst and .map are not generated on my project. Compilation is OK. Could someone send me a running ST7LITE15BF0 project folder with a very little .asm program (set one port to 1 for example)to help me fixing my problem? I wait for your help Regards2007-09-27 9:26 PM
2007-09-27 9:39 PM
Hi_luca,
I'm using the ST7 asembler linker from STVD7 and inDART-STX from SOFTEC. The .cbe error file I get is : ****************************************************************** No errors on assembly of 'C:\Documents and Settings\ST7\TEST PILE\ST7LITE15B.asm' No errors on assembly of 'C:\Documents and Settings\ST7\TEST PILE\testpile.asm' No errors on assembly of 'C:\Documents and Settings\ST7\TEST PILE\ST7LITE15B.asm' C:\Documents and Settings\ST7\TEST PILE\ST7LITE15B.INC(16): as1 : Fatal 79: Couldn't find label list in map file 'testpile.map' ************************************************************************* The message I get when building the project is : ************************************************************************* STMicroelectronics assembler v4.49 No errors on assembly of 'C:\Documents and Settings\ST7\TEST PILE\testpile.asm' C:\Documents and Settings\ST7\TEST PILE>lyn ST7LITE15B.obj+testpile.obj,testpile.cod; STMicroelectronics - Linker - rel 3.16 200K namespace for approx 8150 publics C:\Documents and Settings\ST7\TEST PILE\testpile.asm(66): lyn : Error 5: No information on start address of class 'ram0' C:\Documents and Settings\ST7\TEST PILE>asm ST7LITE15B -sym -fi=testpile.map STMicroelectronics assembler v4.49 No errors on assembly of 'C:\Documents and Settings\ST7\TEST PILE\ST7LITE15B.asm' C:\Documents and Settings\ST7\TEST PILE>asm testpile -sym -fi=testpile.map STMicroelectronics assembler v4.49 C:\Documents and Settings\ST7\TEST PILE\ST7LITE15B.INC(16): as1 : Fatal 79: Couldn't find label list in map file 'testpile.map' C:\Documents and Settings\ST7\TEST PILE>obsend testpile.cod,f,testpile.s19,s STMicroelectronics - Obsend - rel 2.13 Single Segment may not be over 192K bytes - aborted at FEFEFEFF The command: ''build.bat build.bat'' has failed, the returned value is: 6 exit code=6. build.bat - 2 error(s), 0 warning(s)************************************************************************ Any idea on what happens?2007-09-27 11:02 PM
Hi SCo,
I received your file but I've got some problems with the paths in your project ! You can find attached the .cbe error file I get. Regards Whitebull ________________ Attachments : cbe.err : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzZ8&d=%2Fa%2F0X0000000bU1%2Fv_7vcuhHk_fxy4Vbov4.h.QbqlcZ1S15qUAdpKxJRzM&asPdf=false2007-09-28 3:21 AM
Hi SCo,
I tried that as soon as I received your files but it doesn't work. I have recereated a new projet with the SOFTEC STVD7 utilty and now it works ! Compilation is OK, Linkage is OK and I can run a little software on my target board! Just one problem, It works if I doesn't use option bytes! With the inDART-STX clock on the osc1 pin of my LITE15BF0 it works. If I use option bytes to validate the internal oscillator the behaviour become a big mess and the link between InDART and target fall down? Any idea? Regards WhitebullWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.