2003-05-20 9:49 PM
2003-05-18 4:37 PM
Hello Anyboby
ST7Lite2 Current I'm using an ST7lite2 and I need to save as much current as possible without an increase to cost. The LVD detection is taking 0.2mA - Is there a better solution? or should I use a external regulator with low voltage detection (But this will add to the cost of the final production) JOM2003-05-19 3:00 AM
hello,
You can reduce the power consumption by using different power saving modes e.g. halt etc. . Its usage depends up on your application means which peripheral/s you want to use and other configuarations.[ This message was edited by: Ranjeet on 19-05-2003 15:30 ]2003-05-20 9:49 PM
Don't forget also to configure all the unused I/Os as output at 0, to switch off all the unused peripherals, to switch off the ADC between 2 conversions if you don't need continuous conversions,...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.