cancel
Showing results for 
Search instead for 
Did you mean: 

ST7Lite and Superlite

shermantec
Associate II
Posted on June 18, 2003 at 07:58

ST7Lite and Superlite

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
shermantec
Associate II
Posted on June 17, 2003 at 19:06

Hello All ,

My customer is using now the ST7Lite for one of his application and he need an accurate communication between the RS232 and he can't use the calibration so i gave him the ST7Superlite for this application .

1 . Can he write the code in the ST7Lite with the Softec Board and then transfer it to the SuperLite ?

2 . When i can get samples of the ST7SuperLite?

Latino Israel
simonharrison9
Associate II
Posted on June 18, 2003 at 07:58

Hi,

Why can't your customer use the 'FLITE for RS232?

The only problem with the internal RC value is when the supply voltage changes.

I have sw uart running on the 'FLITE0 with no problem

Simon

Anglia

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.