2006-03-07 2:46 AM
2005-08-11 8:20 PM
Dear Al
I already have this kind of problem on one of my application. But I completely change my hardware. I use a voltage regulator with shut down. Then when the voltage decrease below 2v the regulator stop regule and then it start proprely each time. I talk with ST support about this problem, they told that we must have a 20usAlso the pin PA6 must be at high level during reset (see description pin on the data sheet). Regards Mustapha2005-08-12 1:39 AM
Hello Mustapha
we are actually considering a redesign as you suggested. But what do you mean with PA6 must be high? Could you tell me where this is written in the datasheet? Just to be sure: we are talking about ST7FLITE2. Thanks Al2005-08-12 3:03 AM
Dear Al,
Yes I talk about ST7FLITE2, you can see the warning about PA6 page 7 on the data sheet August 2003. Regards Mustapha2005-08-14 8:26 PM
... or on page 13 (Rev.3.0, October 2004):
Caution: During normal operation the ICCCLK pinmust be pulled- up, internally or externally (external
pull-up of 10k mandatory in noisy environment).
This is to avoid entering ICC mode unexpectedly
during a reset. In the application, even if
the pin is configured as output, any reset will put it
back in input pull-up.Regards WoRo
2005-08-15 4:38 AM
Dear Mustapha and WoRo
Thanks for your help! It seems to work now, after we added the pull up. (But we still don't understand why the RESET pin does not work in that case...) Thanks again and best regards Al2006-02-28 9:57 PM
Hi all,
I'm upping this old post because, I'm experiencing exactly the same problem than Al_Capone with an ST7FLITE05M6 microcontroller. I'm using LVD with medium thresold voltage and sometime, at power up, the microntroller don't start and keep stuck. The only way to restart the MCU is to pull down Vdd to GND during several seconds and this problem don't occuer at all power-up sequence. The problem is that I did not respect the recommendation of ST7LITE0 datasheet (Rev 3.0 october 2004) on page 14: ''During normal operation the ICCCLK pin must be pulled- up, internally or externally (external pull-up of 10k mandatory in noisy environment). This is to avoid entering ICC mode unexpectedly during a reset. In the application, even if the pin is configured as output, any reset will put it back in input pull-up.''But I don't know if the MCU can enter ICC mode only at power up reset or power up and power down reset are concerned. The problem is that on my board, ICCCLK pin (PA6) cannot be pulled up, so i'm asked 2 question: 1. if MCU enter in ICC mode, will the hardware watchdog will work and generate an MCU reset to leave ICC mode and restart the software ? 2. is it possible to configure dynamically PA6 pin in order to configure it in pull-up mode in normal time and to leave it floating before each port reading? Thanks a lot in advance for your help.2006-03-07 2:46 AM
Hi,
Power down reset is not concerned, but both cold and hot reset are concerned, i.e cold at power-up and hot reset with the CPU still power supplied. 1.Watchdog is not used in ICC mode. 2.There is no way to configure PA6 to avoid this behaviour because it is the configuration during reset which is taken into account. Best regards LaurentWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.