2007-11-06 12:27 AM
2007-10-05 4:50 PM
When I try to compile with ST7 VD (Cosmic Compiler) with Vista, I get the following errors.
access to default.wed is denied can't create *.cx1 Any ideas?? Thanks Dave P2007-11-06 12:27 AM
Quote:
can't create *.cx1
that is a problem by having no write accress to the temporary used directory - normaly the compiler use the %windows%\temp folder (older compiler versions use root) alternative you can set that - using option cxst7.exe -t make sure you have write access to the pathWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.