2009-07-26 10:35 AM
2009-07-26 10:35 AM
Please help -me
Initializing ST10Flasher.dll Init COM2 at 56000 bauds *LOAD MONITOR-->OK *Dump-->ERROR Description: LoadExternalFlashMonitor: target Not found Select All blocks not creat dump... Error ''target not found''2010-05-16 12:17 PM
Mostrar romanização
I'm also having this problem I believe is the version of the program would have someone younger to be able to send me please I'm on version 2.4
thanks
email.
rmacedorj@oi.com.br
2010-07-06 12:01 PM
The MCU is just not in the BSL mode, check the voltage of PL.04 (must be close to 0) and PL.05 (to +5).
2010-11-16 11:27 AM
I've got this problem too, i'm not sure it was the BSL because when i try to save in format .txt, it run properly ! when i choose format .hex...ive got th error....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.