2005-02-09 12:09 AM
2005-02-09 12:09 AM
Hi.
Im develomping an MP3 player using the source code from ST´s NAND flash memory example. I was actualy rather amased over how much code was needed for a memory stick. My problem is that I need to add a function to the source code. I have understod that I should call my own functions from the appli.c file. But there is no help file / app. note for this source code, therefore Im having truble understanding it. I need to get a mp3 file from the nand flash but doesnt understand which function I should call on from the MAL(?) library. I also need some kind of get filelist function that returns directories and filenames stored in the nand memory. I would appreciate any help. Or links to dokuments and Appnotes clarifying this. Best regards FredrikWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.