2017-06-11 3:05 AM
Hello all
I have an eBay ST-LINK V2 with an STM8S003F3P development board. Following the tutorial I have managed to get the project compiled without errors and set up the debugger options as instructed with the SWIM ST-LINK option. However when I attempt to start the debugger I get the Target Selection dialog which is fine but then the following error.
Starting debug session...
-> Emulator reset (usb://usb)... ** Connection error (usb://usb): gdi-error [40201]: can't access configuration database-> Failed to connect target.
The tutorial did not mention I had to include the header file so is there a database that I am supposed to find. Anybody know where it is or what it is called?
#stm8s003f3p #st-link-v2Solved! Go to Solution.
2017-06-12 12:36 AM
Hi David,
I think this is related to either the version of STVD you have or whether you install STVD or the STLink v2 driver first. I'm sure there is a posting about it somewhere :)
Thanks,
Ian
2017-06-12 12:36 AM
Hi David,
I think this is related to either the version of STVD you have or whether you install STVD or the STLink v2 driver first. I'm sure there is a posting about it somewhere :)
Thanks,
Ian
2017-06-12 4:15 AM
Thanks for the reply Ian. Of course I kept looking while I waited for the post to be approved and I eventually found this.
You will need to open a command prompt in administrator mode. For those that don't know you will find it at
Windows/Start button->All Programs->Accessories->
Right click on 'Command prompt' and select 'run as administrator'
First type this one
Regsvr32 /u 'C:\Program Files (x86)\Common Files\Microsoft Shared\DAO\DAO350.DLL'
And then this one
Regsvr32 'C:\Program Files (x86)\Common Files\Microsoft Shared\DAO\DAO350.DLL'This unloads and then reloads the DAO DLL which fixes the problem nicely. It also assumes you have a standard install of Windows so if you put DAO350.DLL somewhere else then you will have to change the paths.
You might also have to cd \windows\system32 before anything to use regsvr32 but mine defaults to there
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.