2008-03-11 4:51 AM
2011-05-17 12:50 AM
Hi,
I'm trying to generate 44100Hz out of the timer3 PWM output with PCLK 48MHZ. unfortunately, PWM frequency is too slow. here my code: SCU_PCLKDivisorConfig(SCU_PCLK_Div2); SCU_PLLFactorsConfig(192, 25, 2); /* Configure Factors FPLL = 96MHz */ SCU_PLLCmd(ENABLE); SCU_MCLKSourceConfig(SCU_MCLK_PLL); /*init */ /* GPIO4 clock source enable */ SCU_APBPeriphClockConfig(__GPIO4, ENABLE); SCU_APBPeriphReset(__GPIO4, DISABLE); GPIO_DeInit(GPIO4); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Disable; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2; GPIO_Init(GPIO4,&GPIO_InitStructure); TIM_StructInit(&TIM_InitStructure); /* 44.100 KHz generation */ TIM_InitStructure.TIM_Mode = TIM_OCM_CHANNEL_1; TIM_InitStructure.TIM_OC1_Modes = TIM_TIMING; TIM_InitStructure.TIM_Clock_Source = TIM_CLK_APB; TIM_InitStructure.TIM_Prescaler =0x1; TIM_InitStructure.TIM_Pulse_Length_1=0x220; /* Initialize the Timer 0 */ TIM_Init (TIM0, &TIM_InitStructure); TIM_StructInit(&TIM_InitStructure); /* PWM configuration */ TIM_InitStructure.TIM_Mode = TIM_PWM; TIM_InitStructure.TIM_Clock_Source = TIM_CLK_APB; TIM_InitStructure.TIM_Prescaler =0x0; TIM_InitStructure.TIM_Pulse_Level_1 = TIM_HIGH; TIM_InitStructure.TIM_Period_Level = TIM_LOW; TIM_InitStructure.TIM_Pulse_Length_1 =0xff; TIM_InitStructure.TIM_Full_Period =0x300; /* Initialize the Timer 3 */ TIM_Init (TIM3, &TIM_InitStructure); void TIM0_IRQHandler(void) { Pulse +=0x220; TIM_SetPulse(TIM3, TIM_PWM_OC1_Channel,sample); /* Set the TIM0 OC1 value */ TIM_SetPulse(TIM0, TIM_PWM_OC1_Channel, Pulse); /* Clear the TIM OC1 flag */ TIM_ClearFlag(TIM0, TIM_FLAG_OC1); } If there is something I'm doing wrong, please direct me with the right direction (code). Thank you in advance,We’re moving the ST Community to a new platform to give you a better and more reliable community experience.