2005-08-09 9:19 PM
2005-08-07 11:00 PM
I can boot diskonchip from DOS(using DOC1xx.exb.->DOC5xx.exb) successful.
I use dformat program to format doc2000-chips and doses not copy any thing to the doc2000. when I boot from linux, the BIOS halt!,Why?(if TrueFFS working, the BIOS dead) I can boot linux from HardDisk.[ This message was edited by: vehicle007 on 08-08-2005 11:32 ]2005-08-09 9:19 PM
To copy files to DOC, you have to upgrade the firmware also: please use this command under DOS.
dformat /WIN:C800 /S:DOC5EXB You can not boot because you have to configure DiskOnChip as a bootable disk for the OS used. I have attached the Installation manual for the DiskOnChip2000 with Linux OS. ________________ Attachments : APP21.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzBw&d=%2Fa%2F0X0000000bKX%2Fae0IhUbEEQKeETUlrpugERiICAslnNQVbsc00tSGaO0&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.