cancel
Showing results for 
Search instead for 
Did you mean: 

SMOD

kobihaun
Associate II
Posted on May 01, 2003 at 20:13

SMOD

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
kobihaun
Associate II
Posted on May 17, 2011 at 11:53

Hi Every Body

The SMOD bit at UPSD.H is disabled.

When I enable it, the compiler shouts error ''PCON invalid base address''.

How can I enable the SMOD bit in the UPSD.H file?.

Thank you all.

Kobi
joseph2399
Associate II
Posted on May 17, 2011 at 11:53

PCON register is NOT bit addressable, only registers reside on addresses x0 and x8 are bit addressable. Although some compilers can use macros to do the bit manipulation; Keil complier does not support it. You need to OR in the bit you want to set or reset.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.