2008-02-11 2:19 AM
2011-05-17 12:31 AM
We're evaluating the IAR quick start kit which comes with the STR912-sk board with a STR912FW4X cpu. X-tal is running at 25MHZ. When we try to use the PLL to bump the clock rate up to the rated 96MHZ, we seem to break down at speeds above 60-70MHZ.
(SCU_PLLFactorsConfig(48, 25, 1) works, (SCU_PLLFactorsConfig(66, 25, 1) works, (SCU_PLLFactorsConfig(72, 25, 1) stops working Any suggestions? does the prt actually work at 96MHZ?2011-05-17 12:31 AM
Hi Jonny_h,
You must ensure that the PLL factors M, N and P respect the conditions indicated in reference manual (see PLL paragraph 2.4.8) In order to have 96MHz, please use the following values: N= 192 , M= 25 and P = 2. Also you must set the flash read wait states to 2 in order to execute from flash. Best Regards, STARM2011-05-17 12:31 AM
Thanks,
Is the requirement for 2 flash read wait states when running at 96MHZ documented anywhere?2011-05-17 12:31 AM
2011-05-17 12:31 AM
Thanks...
2011-05-17 12:31 AM
Update: Page 23.. it is.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.