2011-10-10 12:47 PM
Hi all,
some piece of code to manage a rotary encoder potentiometer. The model I use is from the chinese market maybe by TREXON. I'll propose both interrupt and polling mode. The interrupt code has been adapted from http://www.arduino.cc/playground/Main/RotaryEncoders and the polling one from http://stackoverflow.com/questions/34735/using-a-rotary-encoder-with-avr-micro-controller. Find also the interrupt handler (just modify the stm8s_it.c code as indicated). The code is a part of a hobby project which is a PLL 2.4GHz signal reference generator. The rotary potentiometer if for making a ''knob'' for such a generator to move the output frequency of the PLL. The project also has a 12 keys keypad and a LCD 16x2 display, which I have already posted. The rotary potentiometer CHA goes into GPIOB.PIN0 and the CHB into the GPIOB.PIN1. Hope it helps. Stefano ________________________ main() { .. .. while(1) { &sharpifdef _POLLMODE_ wheel = (GPIO_ReadInputData(GPIOB) & 0x03); if(dir == 0) { if(wheel == 0x01) dir = 2; else if (wheel == 0x02) dir = 4; else dir = 0; } else if (dir == 2) { if (wheel == 0x01) dir = 2; else if (wheel == 0x00) { // decrease frequency VCOFreq -=100; PLL_SetFreq(VCOFreq); LCD_Cmd(LINE_2); Int2Str(sz_Val, VCOFreq); pos = 7; LCD_Str(sz_Val); dir = 0; } else dir = 0; } else if (dir == 4) { if (wheel == 0x02) dir = 4; else if (wheel == 0x00) { // increase frequency VCOFreq +=100; PLL_SetFreq(VCOFreq); LCD_Cmd(LINE_2); Int2Str(sz_Val, VCOFreq); pos = 7; LCD_Str(sz_Val); dir = 0; } else dir = 0; } else if (wheel == 0x03) { dir = 0; } &sharpelse // INT MODE if (changed) { BEEP_Cmd(ENABLE); VCOFreq = counter; PLL_SetFreq(VCOFreq); LCD_Cmd(LINE_2); Int2Str(sz_Val, VCOFreq); pos = 7; // force cursor position <> 0 to simulate typing a new value from the keyboard LCD_Str(sz_Val); changed = 0; BEEP_Cmd(DISABLE); } &sharpendif ____________________ /** * @brief External Interrupt PORTB Interruption routine. * @par Parameters: * None * @retval * None */ &sharpifdef _COSMIC_ @far @interrupt void EXTI_PORTB_IRQHandler(void) &sharpelse /* _RAISONANCE_ */ void EXTI_PORTB_IRQHandler(void) interrupt 4 &sharpendif /* _COSMIC_ */ { u8 portval; portval = (GPIO_ReadInputData(GPIOB) & 0x03); if ((portval == 0x03) || (portval == 0x00)) { counter-=200; } else { counter+=200; } changed = 1; // this is to tell the main to display the new value } #interrupt #encoderWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.