2006-04-06 10:04 AM
2011-05-17 3:07 AM
Ciao,
I have problems in using the RLINK to program a uPSD3233B on board. I'm able to erase , execute a blank test, and on a programmed part execute the verify, but when I try to program it I always get the following error: PSDsoft Express 8.30 Copyright (C) 1993-2004 STMicroelectronics, Inc. All Rights Reserved. DATE : 06/15/2005 TIME : 12:22:24 Device 1 : ( 4 pins ) Program ... Erasing ... Programming/Verifying... fail Program/verify operation unsuccessful ... ERROR: Data (0600) Hint: Programming failure. Time elapsed : 6 sec. By the way, if I use the Flashlink on the same board, I've no problems. I also changed the Rlink, assuming it was damaged, but no changes. Any idea? Thanks2011-05-17 3:07 AM
I am getting this same problem. I can't explain why. The osf file is created correctly. I am using a PSD4256G6V.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.