2006-12-07 5:11 AM
2006-12-07 2:23 AM
Hi all,
I am using an ST7FLITES5Y0 with STVD7 3.3.3. I have programmed the hardware watchdog option, and despite setting the IDE to ignore option bytes the device will not program. When I tell the IDE to use the option bytes I get the known warning about the hardware watchdog. When I tell it to ignore the bytes it ''fails to download monitor''. Both problems only manifested after setting the hardware watchdog. I am using one of the 'new' RLinks. I can't work out where the problem is!2006-12-07 5:11 AM
Sorry boys
I've got a confobulator board with the target board and I think the pinout may be incorrect.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.