2005-10-27 8:02 PM
2005-08-04 6:12 AM
Hello,
Does anybody know the reset value of: - PC0 - PC1 - PC2 - PD THX Manu2005-08-04 10:57 PM
Port 0 :
PC0 = 0xffff PC1 = 0xffff PC2 = 0x0 PD = 0xe0ff Port 1 : PC0 = 0xffff PC1 = 0xffff PC2 = 0x0 PD = 0xfcff Port 2 : PC0 = 0xffff PC1 = 0xffff PC2 = 0x1 PD = 0xff0f These are the values that can be derived from the Reference Manual, if I'm understanding it correctly. (On my STR711, however, it seems that P0.15 is configured for TTL input at reset. This is not mentionned in the docs.) Can anybody at ST confirm the values ?2005-08-04 11:05 PM
Thank you,
where did you find the reset value in the reference manual ? (I didn't find it, there's just an asterisk)2005-08-05 12:10 AM
The values are not explicitely written in the Reference Manual, but you can calculate them using the information in the Device Pin Description table (see page 22).
2005-08-05 12:19 AM
OK, thanks
2005-10-27 8:02 PM
Hi,
Can someone confirm the pin configurations upon reset here? Rgrds, ongth60We’re moving the ST Community to a new platform to give you a better and more reliable community experience.