2003-11-24 4:51 AM
2003-11-24 3:01 AM
hi !
when i use the output compare function , when i'm writing to the CLR register will it reset the counter ???? thanks. adi2003-11-24 3:08 AM
Which device are you using??
2003-11-24 3:17 AM
st72264
2003-11-24 3:56 AM
Yes, while using 16-bit timer/output compare function , the counter is reset by writing into the count low register(CLR). It is also mentioned into the datasheet.
2003-11-24 4:51 AM
yes ,it is written in the datasheet but not under the output compare function section and i just wanted to be sure.
thanks.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.