2024-05-20 2:42 AM
Hello, I'm Jade.
We are using ST Micro's M24C04 parts.
I bought the parts, but the shape of the imprint is different, so I'm inquiring about which one is real.
Please refer to the picture below. Lot information is the same, but ST mark is different.
Thank you
2024-05-21 3:55 AM
Welcome @JadeYoon, to the community!
The labelling does indeed look very strange. However, you cannot definitively conclude from this that it is fake device.
If you have a sticker on the packaging with a bulk ID on it, you are welcome to send me a legible photo via PM so that I can check it. However, please do not post it here in the community to avoid abuse.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.