2003-08-28 8:31 PM
2011-05-17 2:55 AM
Hello,
1. I am trying to connect a switch to PB4 on the DK3 I have made the necessary changes in the configuration for Port B and in the PSD soft, confiugred the pin to be GPIO. Also i have a 4.7K resistor pullup for PB4 to Vcc2. But still i am not able to get any response from the switch. I am able to use the other switches ( SW4 & SW5 ) which are connected to pins of Port B. 2. Can i access the Port B from the timer ISR ? I want to read the switch status at a regular interval, and glow the corresponding LED's from timer0 ISR. If i put the code outside timer routine, i am able to do it, but not from timer0 ISR. Kindly suggest me how to go for the above problems. Regards, Bhushan.2011-05-17 2:55 AM
Can you post the *.abl file in the formus
2011-05-17 2:55 AM
Hi,
Here is the *.abl file module trial1 LCD_d7 PIN 21; ''Reserved for Peripheral I/O mode LCD_d6 PIN 22; ''Reserved for Peripheral I/O mode LCD_d5 PIN 24; ''Reserved for Peripheral I/O mode LCD_d4 PIN 26; ''Reserved for Peripheral I/O mode LCD_d3 PIN 28; ''Reserved for Peripheral I/O mode LCD_d2 PIN 32; ''Reserved for Peripheral I/O mode LCD_d1 PIN 34; ''Reserved for Peripheral I/O mode LCD_d0 PIN 35; ''Reserved for Peripheral I/O mode LCD_enable PIN 66; LCD_rw PIN 67; LCD_rs PIN 72; SW3 PIN 73; ''GP I/O SW2 PIN 74; ''GP I/O SW1 PIN 76; ''GP I/O LED2 PIN 78; ''GP I/O LED1 PIN 80; ''GP I/O tdo PIN 6; ''TDO tdi PIN 7; ''TDI vbaton PIN 9; ''Standby-on indicator vstby PIN 15; ''SRAM standby voltage input tck PIN 16; ''TCK tms PIN 20; ''TMS ale PIN 4; ''ALE output SCL2 PIN 46; ''I2C bus - Clock SDA2 PIN 44; ''I2C bus - Data ADC_Ch0 PIN 59; ''ADC channel0 input Toggle_pin1 PIN 52; ''GP I/O a11 PIN 57; ''Address line a10 PIN 55; ''Address line a9 PIN 53; ''Address line a8 PIN 51; ''Address line a7 PIN 47; ''Data/address bus line a6 PIN 45; ''Data/address bus line a5 PIN 43; ''Data/address bus line a4 PIN 41; ''Data/address bus line a3 PIN 39; ''Data/address bus line a2 PIN 38; ''Data/address bus line a1 PIN 37; ''Data/address bus line a0 PIN 36; ''Data/address bus line _Reset_In PIN 68; VREF PIN 70; ''VREF input _rd PIN 62; _psen PIN 63; _wr PIN 65; USB_minus PIN 8; ''USB- bus USB_plus PIN 10; ''USB+ bus Xtal1 PIN 48; ''Xtal1 Xtal2 PIN 49; ''Xtal2 psel0 node; rs0 node; csiop node; fs0 node; fs1 node; fs2 node; fs3 node; csboot0 node; csboot1 node; csboot2 node; csboot3 node; _reset node 543; a12 node 512; a13 node 513; a14 node 514; a15 node 515; pgr1..pgr0 node; X = .x.; address = [a15..a0]; page = [pgr1..pgr0]; Vcc = 1; Gnd = 0; // Begin user preserved declarations (not affected by iterations of DA usage) =================== // End user preserved declarations (not affected by iterations of DA usage) =================== equations rs0 = ((address >= ^h2000) & (address <= ^h3FFF)); csiop = ((address >= ^h0200) & (address <= ^h02FF)); fs0 = ((page == 0) & (address >= ^h8000) & (address <= ^hFFFF)); fs1 = ((page == 1) & (address >= ^h8000) & (address <= ^hFFFF)); fs2 = ((page == 2) & (address >= ^h8000) & (address <= ^hFFFF)); fs3 = ((page == 3) & (address >= ^h8000) & (address <= ^hFFFF)); csboot0 = ((address >= ^h0000) & (address <= ^h1FFF)); csboot1 = ((address >= ^h2000) & (address <= ^h3FFF)); csboot2 = ((address >= ^h4000) & (address <= ^h5FFF)); csboot3 = ((address >= ^h6000) & (address <= ^h7FFF)); psel0 = ((address >= ^h0300) & (address <= ^h03FF)); LCD_enable = ((address >= ^h0300) & (address <= ^h03FF) & (!_rd)) # ((address >= ^h0300) & (address <= ^h03FF) & (!_wr)); LCD_rw = a0; LCD_rw.oe = Vcc; LCD_rs = a1; LCD_rs.oe = Vcc; // Begin user preserved equations (not affected by iterations of DA usage) =================== // End user preserved equations (not affected by iterations of DA usage) =================== end trial1 Bhushan.2011-05-17 2:55 AM
Your ABL file is correct. I think you would check your circuit and check if the PB4 is low when the key is pressed.
Now you read the PB data IN register (csiop + 01).2011-05-17 2:55 AM
There is good example of how to use PB port and SW1 & SW2 int the following attachment.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.