2004-04-01 12:35 AM
2004-03-31 3:26 AM
Hi all,
I have to bother you one more time with questions about the readout protection byte. Basis: A blank ST7Flite25 is first time programmed with STVP 1.9.1 in the DIL20 socket , on the ST7MDT10-EPB eval board. The option byte: readout protection is set ON. Is it possible to ever reprogramme it, with above tools ? 1. When using the internal RC oscillator in the final application ? 2. When using an external crystal in the final application ? If so - how ( step by step please )? Any other tools making this possible ? Regards, Tomas2004-03-31 10:18 PM
Yes, you can reprogramme the read out protection option bytes.
Procedure is : 1. First using STP7, first program the option bytes with Read out protection setting - OFF. 2. Step1 will also erase your program memory(the STP7 1.9.1 does n't erase the internal RC calibration values). Reprogram your program your memory. 3. Now, you can reprogram the desired/new option bytes. [ This message was edited by: Jatin on 01-04-2004 11:49 ]2004-04-01 12:35 AM
Hi Jatin,
fast and accurate as always ! By misstake earlier I tried to set the option byte OFF, but I used ''program all tabs'' instead of ''program current tab''. That's the way is goes for an OTP-oldie coming from ST62.... Many thanks ! Best regards, TomasWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.