2008-03-28 7:43 AM
2011-05-17 2:52 AM
Hello,
I use a UPSD3354DV-40u6 and have a problem with reading the internal SRAM. After testing several pcb boards the result is that I have boards that read corrupt data from the internal SRAM. After debugging I have seen that a wrong board has a ''bad signal'' at the databus when reading at an adres in SRAM. With ''bad signal'' I mean that it is not a nice ''1'' but a slow rising signal from ''0'' to ''1'' like loading a capacitor. Other external busdrivers can drive the bus and are tri-state at the moment the SRAM is reading. (seen with a scoop that triggerd on the \RD pin an looking at MCUAD0 (multiplexed databus 0)). After some testing the board is working fine and it have a good signal. Please let me know if you have some tips or suggestions to solve this problem. Best regards, André2011-05-17 2:52 AM
Hello all,
The problem is solved. The reasen was that the battery voltage (PC2) was sometime above the Vdd so thhe SRAM goes in protection mode. Best regards, AndréWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.