2006-03-10 4:36 AM
2011-05-17 3:06 AM
How do I do this in PSDSoft Express?
How do I erase the Flash in PSDSoft Express? I am jumping two pins together to erase the flash memory, when the pins are equal, then i want the flash to erase.2011-05-17 3:06 AM
I am working the first time with the upsd3254A and I can't understand how to read and write data from the Flash.
Has anybody some easy examples for me, how I could do this. It would be really helpful! I have the same problem with the SRAM. I don't really understand the text in the datasheet about the Flash and the SRAM. I hope somebody could helb me! regards Xaver2011-05-17 3:06 AM
hi,
this is simple: - set the adress-ranges for the flash-sectors/sram in PSDflash. (i.e. for SRAM: 0x000 ... 0x1FFF) - read SRAM: MOV DPTR,#0000h ;read 1st byte in SRAM MOV A,@DPTR MOV DPTR,#1234h ;read byte at address 1234h from SRAM MOV A,@DPTR - write SRAM: MOV DPTR,#1234h ; MOV @DPTR,A - read flash: exactly like SRAM - write flash: this is a bit more complicated (but also completely described in the datasheet)2011-05-17 3:06 AM
Quote:
On 09-05-2005 at 20:23, Anonymous wrote: hi, this is simple: - set the adress-ranges for the flash-sectors/sram in PSDflash. (i.e. for SRAM: 0x000 ... 0x1FFF) - read SRAM: MOV DPTR,#0000h ;read 1st byte in SRAM MOV A,@DPTR MOV DPTR,#1234h ;read byte at address 1234h from SRAM MOV A,@DPTR - write SRAM: MOV DPTR,#1234h ; MOV @DPTR,A - read flash: exactly like SRAM - write flash: this is a bit more complicated (but also completely described in the datasheet) You surely can't MOV A,@DPTR and similar. The flash and SRAM act as an external memory with a conventional 8051. It's mapping depending on the DPLD (defined as ''address-range'' in PSDSoftExpress) and the status of VM register (it's default state after reset defined by the setting in PSDSoftExpress as ''Main/Secondary mamory will reside... program/data space'' in the ''Define PSD and MCU/DSP'' step; runtime modified by writing into VM register in the register space). So you can have mapped the primary/secondary flash and SRAM as program memory only, both program and data memory and data memory only. The rules to access them are - again - the same as with conventional 8051 and appropriately mapped external memory. If the memory is accessible as program memory, you can't write, only read using the MOVC A,@A+DPTR and MOVC A,@A+PC commands (and of course run program from it)(see any 8051 reference book, or the ''bible'') . To read from data memory mapped flash/sram, use MOVX A,@DPTR or MOVX A,@Rn commands. Writing to SRAM is using MOVX @DPTR,A or MOVX @Rn,A; but - as correctly said above - writing to FLASH is more complicated, search for IAP in this forum. Jan WaclawekWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.