2008-02-11 5:11 AM
2008-02-11 2:00 AM
Hi
Just starting to use th ST7 Lite Ultra 09, the data sheet states that the calibration data is 10 bit and held in memory DEE0 (hi Byte) and DEE1 (lo byte) The 2 bits of the lower byte shares the SICSR register in assembler how should I read the calibration and set the SICSR & RCCR. Regards, Brian2008-02-11 5:11 AM
Hi Brian
Use this: ; ; Clock ; 10 Bit RCCR to load ; Option Byte: CKSEL[1:0] = 00 ; .ini_st7 ld A, $DEE2 ; Calbration value (Special Bytes outside Flash) ld RCCR, A ; set to 8 MHz @ 3.3 Volts @ 25°C CR[9:0] ld A, $DEE3 ; and A, #%01100000 ld SICSR, A ; CR[1:0] More precise information You can find in the FOXU... data sheet: 1. The DEE0h and DEE1h addresses are located in a reserved area in non-volatile memory. They are readonly bytes for the application code. This area cannot be erased or programmed by any ICC operations. For compatibility reasons with the RCCRL register, CR[1:0] bits are stored in the 5th and 6th position of DEE1 address. Kind regards hansjuschWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.