2017-02-22 5:08 PM
Hi
I am using 20 pin STM8s003f3 controller. I have programmed TIM2 channel 3(pin 10) in Input capture mode with capture to be made on falling edge detection on channel 3. I have enabled TIM2 capture/compare interrupt. I have also configured the option byte.
I am facing problem related to interrupt, there is no pulses or signals at channel input but still execution goes into the interrupt repeatedly. I am not getting what is problem. Please see below TIM2 initialization and interrupt code.
//TIM2 Initialization
TIM2->PSCR = 0x04; //Deviding incoming clock by 16 Fck_cnt = Fck_psc/(2^PSC[3:0]);
TIM2->CCMR3 |= 0x01; //CONFIGURING CHANNEL IN INPUT CAPTURE MODE TIM2->CCMR3 |= 0x10; //INPUT SAMPLING UPTO TWO CLOCK CYCLES TIM2->CCER2 |= 0x02; //SELECTING FALLING EDGE AS TRIGER SIGNAL TIM2->CCER2 |= 0x01; //ENABLED CAPTURE INPUT TIM2->IER |= 0x08; //CAPTURE/COMPARE INTERRUPT IS ENABLED TIM2->CR1 |0x01; //TIM2 ENABLEDINTERRUPT_HANDLER(TIM2_CAP_COM_IRQHandler, 14)
{ GPIOD->ODR ^=0x10; //Toggling PD4 TIM2->SR1 &= 0xf7; //clearing Capture flag}I am using STVD for program development. Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.