2005-10-16 10:58 PM
Problems with the ST10F269 Programmer Tool ST10 Flasher 2.02
2005-10-04 10:38 PM
Hello,
my name is sebastian and I'm from germany (munich). I'm working with the Keil Compiler Version 3 The processor I want to programming is the ST10F269. I connect my processor board over serial to the pc. Ok... When the Coding of my application is done, so I want flash it into the ROM. So... I start the ST10 Flasher :) and then I choose the hex File I want to flash into the ROM. After choosing the following message is shown.. ''Remap first Segment your code use Flash in both segments 0 and 1. Only one of them can be programmend. Which one? [] Segment 0 [] Segment 1 '' BUT in the Assembler File StartST10.a66 from Keil... the ''Segment-Choose-Bit'' ROMS1 is set to zero... so the programm shouldn't ask... but it did.... So I had choosen one the segments (for test I had choose first one and then the other) But the programming wasn't succesfull. Who can help me??? Thanks :)2005-10-06 9:44 PM
Hello,
thanks for your answer! What do you mean by the ''programming wasn't succesfull''. You're right that the message ''Program Flash --> OK '' after programming was shown. But the first print instruction in my main application wasn't accomplished, so I'm sure that the ROM was successfully flashed. In my compiler options I set the following things: - L166 Locate: [x] use memory layout from target dialog Target Classes: ICODE (0x0-0x7FFF), NCODE (0x20000-0x2FFFF), FCONST (0x0-0x7FFF, 0x18000-0x4FFFF), HCONST (0x0-0x7FFF, 0x18000-0x4FFFF), XCONST (0x0-0x7FFF, 0x18000-0x4FFFF), NCONST (0x4000-0x7FFF), NDATA (0x100000-0x103FFF), NDATA0 (0x100000-0x103FFF), SDATA (0xC000-0xE7FF, 0xF600-0xFDFF), SDATA0 (0xC000-0xE7FF, 0xF600-0xFDFF), IDATA (0xF600-0xFDFF), IDATA0 (0xF600-0xFDFF), FDATA (0x100000-0x17FFFF), FDATA0 (0x100000-0x17FFFF), HDATA (0x100000-0x17FFFF), HDATA0 (0x100000-0x17FFFF), XDATA (0x100000-0x17FFFF), XDATA0 (0x100000-0x17FFFF) Target: External Memory: #1 RAM Start: 0x100000 Size: 0x80000 I don't understood why this segment message is every time shown when I want to flash my program. regards, Sebastian2005-10-16 10:58 PM
But the first print instruction in my main application wasn't accomplished, so I'm sure that the ROM was successfully flashed.
I had an error in my last message... I mean that I'm sure that the ROM was NOT successfully flashed... after this ''segment-message''... I'm still... helpless... :(We’re moving the ST Community to a new platform to give you a better and more reliable community experience.