2011-09-07 6:38 AM
When the JP instructions jump less than 92H I haven't any problem, but if it jumps more than 92H the JP and Call command do not work properly. I am sure to be in the same section because I use STM8S105C6.
Example1: 0x80E8 jp Base if the label Base is an address 0x8110 the compiler translates in JP 0x8110 >>Correct if the label Base is an address 0x8181 the compiler translates in JP 0x8081 >>Wrong if the label Base is an address 0x8259 the compiler translates in JP 0x8159 >>Wrong if the label Base is an address 0x8349 the compiler translates in JP 0x8149 >>Wrong if the label Base is an address 0x83B5 the compiler translates in JP 0x80B5 >>Wrong Example2: 0x83DD jp Base2 the label Base2 is an address 0x8685 the compiler translates in JP 0x8085 >>Wrong After 0x817B every label must have the ''.w'' suffix for ex: Base.w The call instruction is the same. Why? Did I forget a few assembler directives? Thanks2011-09-07 6:53 AM
try JPF/CALLF instructions
2011-09-07 10:34 AM
Already tried is the same
2012-01-31 6:20 AM
The same problems there are with the STVD ver. 4.3.0.
If there are some errors during compiling the STVD ver. 4.3.0 go to crash. There is a bug?2012-02-15 5:33 AM
Hi Marco,
also to me it happens: STVD 4.3.0 crashes when it founds errors. With STVD 4.3.1 they corrected this problem but I found another problem about SWIM communication when starting debug, so I'm actually using STVD 4.2.0 , because it's the only that works fine!!2012-03-01 4:07 AM
Solved
It was necessary before '' segment 'rom' '' write WORDS. With this word the problems go away.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.