2005-05-01 10:32 AM
Problem with ST72F521 internal RC oscillator
2005-04-28 10:33 PM
Hello,
I am using the internal RC ocsillator as the main clock of the ST7 and the frequency is supposed to be around 3MHZ. However, i measured the ST7's frenquency at 300HZ!!!! To mesure this frequency, I used the INdart usb card to flash the ST7 and i wrote a progam wich did a simple loop of 3600 cycles . I set a bit defore the loop, i reset it at the end of the loop and I check it with the oscilloscope. I though that a simple reset of the ST7 would set the frequency correctly... (I connected both output OSC1 and OSC2 to the ground as it is written in the datasheet....) How can I do to set the frequency at 3MHZ? thanks a lot for helping me, sincerely2005-04-29 10:05 PM
I solve the problem!!!
If you are using breakpoint to debbug your program, the soft (for inDartUSB card) write a big additionnal program in the component so after the component goes really slow (300HZ instead of 1,5MHZ). Do not used breakpoint to debug it. Now it is working but i still do not understand why the difference is so big. Thanks I hope it would help some of you.2005-05-01 10:32 AM
As you can find on SofTec Microsystems FAQ page:
This happens when your target device doesn't feature the on-chip debug module. In this case, step commands are not executed in real time, for a series of reasons which are explained in detail in the user's manual addendum.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.