2006-03-14 11:54 PM
2006-03-13 9:38 PM
Hi,
I can't set the P0.10 gpio pull up internal resistor. I'm using the STR710 library and the following code: //set the P0.10 in pull up/ pull down weak input mode GPIO_CONFIG(GPIO0, 0x0400, GPIO_IPUPD_WP); //Set the pull up resistor GPIO_BITWRITE(GPIO0, 10, 1); NB : I'm using a raisonance evaluation card with a str712f microcontrollers. Thanks.2006-03-14 11:46 PM
P0.8 and P0.10 are ''true'' open drain rather than being push pull.
I put the question to ST about P0.8 and they indicated that the week pull up is NOT available on this pin (as part of it's 5V tolerance I believe). The doco does not advise that weak pull up is not available. Even after you move it to another pin be careful. If you use the library, when you change a different output pin on the same port you can change your pull ups to pull downs. This is because they do a read modify write on the port data register. When it is read it reads the INPUT state and when you write it back it sets the pull down polarity.2006-03-14 11:54 PM
thanks a lot for these informations.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.