2007-04-20 2:41 PM
power LED off when connecting Jlink!?
2007-04-20 3:19 AM
STR750-SK/IAR is used,
set jumper to EXT power, connect 9V DC to power jack, the power LED is on and message displayed on LCD panel but when I connect Jlink to the board, the power LED is off!? any idea what happened? note that there is no problem with this Jlink connect to STR710-SK/IAR and external 9V DC supply!2007-04-20 1:55 PM
I connect 9V DC with jumpper set to EXT,
then connect Jlink, and the power LED goes off, and I execute the Jlink.exe the message reply in DOS prompt are SEGGER J-LINK Commander V3.10b ('?' for help) Compiled Feb 9 2006 20:21:29 Can not connect to J-Link via USB J-Link>2007-04-20 2:01 PM
Sorry for my careless,
I forget to connect Jlink to PC with last action, now the message replied with executing jlink.exe are SEGGER J-Link Commander V3.10b ('?' for help) Compiled Feb 9 2006 20:21:29 DLL version V3.10b,Compiled Feb 9 2006 20:21:16 Firmware : J-Link compiled Feb 8 2007 10:49:18 ARM Rev.5 Hardware : V5.40 S/N :15400606 OEM : IARKS Vtarget - 0.000V Speed set to 30 kHz J-Link>2007-04-20 2:32 PM
I measure the Jlink pin 19 (connect Jlink to PC USB) , but no 5V out put as it should be !?
any action to activate the Jlink pin 19 voltage output?2007-04-20 2:41 PM
sorry for all the mess ,
the Jlink is mis connect to the AIN connector to cause the problem !We’re moving the ST Community to a new platform to give you a better and more reliable community experience.