2004-03-10 9:36 PM
2004-03-09 2:44 AM
Hi,
I work on ST10F168 with 6M*16bits external ram. This external Ram is used by the microcontroller and a xilinx, so the datas and adress bus are divided by 2 chips. I would to know if i can put POL & POH & P1L & P1H & P4 in tristate mode when the xilinx is accessing external Ram. Can i do this manually by software or using HOLD,HLDA,BREQ signals with logic combination? I see this signals work automatically but i don't know if it work with another chip. If it can, how does it work? Thanks Regards, Jim2004-03-10 9:36 PM
Hello,
The bus arbitration mechanism can work with any other chip. See the attached pdf pages extract from the ST10F269 user manual. ________________ Attachments : Bus_arbitration.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0OP&d=%2Fa%2F0X0000000bYR%2FBMoyXuq2HoGirzkKUMYXrKVqwBlUmDOq2tO0ArYUvkc&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.