2025-08-20 11:44 PM - last edited on 2025-08-21 7:19 AM by Peter BENSCH
Could you please suggest a PLC module that includes a signal scaling unit and an isolation circuit, equipped with a high-speed sampling ADC with up to 16-bit resolution? The module should also integrate a microcontroller featuring SPI, LAN (Ethernet), SD card storage, and an HDMI port.”
Solved! Go to Solution.
2025-08-21 7:19 AM
Welcome @rakesh1184, to the community!
What do you mean by PLC – Power Line Communication or a Programmable Logic Controller?
In both cases, however, STMicroelectronics does not offer ready-made modules. For these, you will need to contact the relevant manufacturers.
Regards
/Peter
2025-08-21 7:19 AM
Welcome @rakesh1184, to the community!
What do you mean by PLC – Power Line Communication or a Programmable Logic Controller?
In both cases, however, STMicroelectronics does not offer ready-made modules. For these, you will need to contact the relevant manufacturers.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.