2004-06-06 7:16 PM
Pin Function changes from in to out ??!!
2011-05-17 3:01 AM
there is a strange behavior:
a porta pin configurated as logic input changes to output and toggles each 50 to 500ns. i do not write to the csiop-register via my progcode. is there any errata sheet for the 3233B ? thanks in advance !!2011-05-17 3:01 AM
Port A works fine.
Go back to your PSDsoft project and check your selections for the Port A pin in question. I suspect you have selected a pin function that you don't desire.2011-05-17 3:01 AM
port a4 is cpld input in psd express:
logic or address but changes to output sometimes ?! what if i define it as input in psd express and overwrite this settings with my soft changing the port a direction via csiop+02 or csiop+06 ???? will i overwrite the psd express settings? thanks again !!!!!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.